REACH & RoHS and Product Carbon Footprint

The use of hazardous substances in products is subject to ever-stricter international laws and restrictions.

To process your enquiry, we would therefore like to provide you with the following information: the products we deliver to you do not, to the best of our knowledge, contain any substances in concentrations that would prohibit their placing on the market.

The regulations in question meet the following legal requirements, among others:

  • 2011/65/EU: RoHS Directive
  • 1907/2006/EC: REACH Regulation
  • 2006/122/EC: Directive on the restriction of perfluorooctane sulfonates ("PFOS")
  • 1005/2009/EC: Regulation on substances that deplete the ozone layer
  • ElektroStoffV: Regulation on electrical and electronic equipment substances
icon POP – Regulation (EU) No. 2019/1021 of the European Parliament

Product Carbon Footprint

We have calculated the product carbon footprint (cradle-to-gate) for a large number of our products. If you are interested, please contact us directly.

icon Find out more

RoHS Directive 2011/65/EU of the European Parliament

Directive 2011/65/EU of the European Parliament and of the Council of June 8, 2011, on the restriction of the use of certain hazardous substances in electrical and electronic equipment

Directive 2011/65/EU (RoHS II) restricts the use of lead, cadmium, mercury, hexavalent chromium, polybrominated biphenyls (PBBs) and polybrominated diphenyl ether (PBDEs) in certain electrical and electronic equipment (EEE). In July 2011, this directive came into force and completely replaced the old Directive 2006/95/EC (RoHS) as of 3 January 2013.

No new substances have been added to the list of prohibited substances in RoHS II. However, the restrictions are no longer limited to the existing substances, but rather a process has been introduced to add additional substances in the future (similar to REACH). LAPP will continue monitoring the process and respond to possible further restrictions on substances.

Regardless of the scope of the RoHS II Directive, all products in LAPP's main catalogue comply with Directive 2011/65/EU (RoHS II) on the restriction of the use of certain hazardous substances in electrical and electronic equipment. These products do not contain any of the prohibited substances specified in the RoHS II Directive or the maximum permissible concentrations specified therein, taking into account the exceptions listed in Annex III of the directive.

Important change to the exemptions (6) of the EU RoHS Directive

In the EU Official Journal in November 2025, the EU Commission decided to change important exemptions for lead in steel, aluminium and copper and in some cases to no longer extend them. Narrower limits for use have been added for several exceptions.

Exemption 6c (lead as an alloy component in copper) will only be extended to a limited extent.

A further extension is possible, but unlikely. If there is no further extension, no more products with this exemption may be placed on the market from 30 June 2027.

REACH – Regulation (EC) No. 1907/2006 of the European Parliament

Regulation (EC) No. 1907/2006 of the European Parliament and of the Council of 18 December 2006 concerning the Registration, Evaluation, Authorization and Restriction of Chemicals

With the REACH Directive, the EU created a harmonised system for the registration, evaluation, authorisation and restriction of chemicals – referred to as REACH for short. The purpose of the directive is to ensure a high level of protection for human health and the environment.

Customer information

Toxic Substances Control Act (TSCA)

On 5 February 2021, the U.S. Environmental Protection Agency (EPA) published a new rule under Section 6 of the Toxic Substances Control Act (TSCA), according to which 5 PBT substances should be banned in products in the USA at short notice, subject to various exceptions. The list of substances banned for import, processing (manufacturing) and sale in products in the USA as of 8 March 2021 is as follows:

  • decabromodiphenyl ether (DecaBDE) (CAS No. 1163–19–5)
  • phenol, isopropylated phosphate (3:1) (PIP (3:1)) (CAS No. 68937–41–7), other names: Tris (4-isopropylphenyl) phosphate; CAS: 68937-41-7]
  • 2,4,6-Tris(tert-butyl)phenol (2,4,6-TTBP) (CAS No. 732-26-3)
  • hexachlorobutadiene (HCBD) (CAS No.87–68–3)
  • pentachlorothiophenol (PCTP) (CAS No.133-49-3)

After inspecting the information available to us, we found that 4 of the 5 substances are also part of the GADSL list and are therefore already subject to declaration by automotive suppliers. Further information about the substances, areas of use and their restriction in the USA can be found under TÜV SÜD – USA: EPA bans five PBT chemicals and EPA: Assessing and Managing Chemicals under TSCA.

icon EPA information on PBT chemicals

Due to the current situation and the upcoming US ban, we are currently actively working on checking our products and materials for the presence of the specified substances. However, as this is a short-term legislative adaptation in the USA, we are not in a position to provide a definitive stance here at this time.

As soon as reliable information is available, we will respond to your enquiry accordingly.