Skip to content
Lapp Asia Pacific SG
Spend SGD 1,200 more for FREE shipping.
FREE shipping will be applied at checkout

Your cart is empty

Continue shopping
0Cart(SGD 0.00)

Industry-Specific Connectivity Glossary

The world of industrial connectivity is vast, with specialized terms that vary by sector. Understanding these niche terms is key to ensuring your systems are reliable, compliant, and cost-effective.

This modular glossary breaks down essential connectivity terms by industry, helping you quickly grasp the concepts that matter most to your specific operations.

Renewable Energy Connectivity Glossary

In solar farms, wind turbines, and energy storage systems, cables and connectors face unique challenges like extreme UV, temperature swings, and direct burial. Here are the terms that ensure your renewable energy project generates power reliably for decades.

For Solar Project Developers & System Installers

These terms are crucial for the design, procurement, and installation of solar photovoltaic (PV) systems.

Term A Simple Definition Why It Matters for Your Project
Solar Cable (PV Cable) A specialized solar pv  cable designed to connect solar panels, inverters, and combiner boxes. It’s built for outdoor use. Standard electrical cables won’t survive the brutal outdoor environment. Solar cables like ÖLFLEX® SOLAR are UV-, ozone-, and temperature-resistant, ensuring decades of reliable power generation and preventing premature cable degradation.
Combiner Box An enclosure where multiple solar string cables are brought together before connecting to an inverter. This box consolidates wiring, often including surge protection and fuses. Proper cable management and durable, sealed connections inside are vital for safety, isolating faults, and maximizing system efficiency.
String Cable The cable that connects a series of solar panels (a “string”) to a combiner box or directly to an inverter. These cables carry DC and are constantly exposed to the outdoor challenging elements. Their durability directly impacts the long-term performance and safety of your solar pv array.
Inverter (PV Inverter) A device that converts the direct current (DC) electricity from solar panels into alternating current (AC) for the grid or consumption. Reliable cabling to and from the inverter is crucial. Specialized DC and AC cables ensure maximum power transfer, minimal energy loss during conversion, and safe grid interconnection.
MC4 Connector A common, waterproof, snap-together connector used to link solar panels together and to solar cables. These are the most widely used connectors in solar PV. Using high-quality MC4 connectors like EPIC® SOLAR ensures a secure, weatherproof connection, preventing hot spots and dangerous arc faults.
TÜV Certified A certification mark from German technical inspection associations (TÜV) confirming a product meets safety and quality standards. For solar pv components, TÜV certification is a stamp of quality and reliability. It assures that your cables and connectors meet rigorous international standards for performance and safety in challenging outdoor conditions.
IEC Standards (International Electrotechnical Commission) Global standards for electrical and electronic technologies, including specific standards for solar and wind components. Adherence to IEC standards (e.g., IEC 62930 for PV cables, IEC 61400 for wind turbines) ensures interoperability, reliability, and safety across international markets, especially for utility-scale projects.
Grounding/Bonding Cable Cables used to create a low-resistance path to earth for electrical current, connecting metal components to a grounding electrode. Essential for safety in solar pv installations, protecting personnel from electric shock and equipment from surges. Proper grounding prevents voltage build-up and provides a path for fault currents.
Rapid Shutdown A safety device in solar PV arrays that quickly reduces voltage to safe levels, typically at the module level, during emergencies (e.g., firefighting). Specific cabling and connectors are required for these devices to ensure they can reliably de-energize the array quickly, protecting first responders and property.
SPD Cabling (Surge Protection Device Cabling) The cables that connect surge protection devices (SPDs) within an electrical system. Proper cabling to and from SPDs is critical. These cables must be short and correctly routed to effectively divert damaging surge (from lightning or grid events) away from sensitive equipment or systems

For Wind Turbine Engineers & Operators

These terms address the unique challenges of wind power, including extreme motion, height, and harsh weather conditions.

Term A Simple Definition Why It Matters for Your Project
Torsion-rated Cable A cable specifically designed to withstand repeated twisting motions along its axis, without internal conductor breakage. Wind turbines’ nacelles (the housing at the top) twist constantly to face the wind. Standard cables would quickly fail. Torsion-rated cables ensure continuous power and data flow from the nacelle to the tower base.
Tower Cable The main power and data cables running vertically inside the wind turbine tower, connecting the nacelle to the grid connection. These long cable runs must be robust enough to handle the turbine’s internal environment, including potential vibrations and temperature fluctuations, ensuring efficient power transmission down the tower.
Slip Ring An electromechanical device that allows the transmission of power and electrical signals from a stationary to a rotating structure. Slip rings are used where cables can’t twist indefinitely. Cables connecting to a slip ring must be designed for frequent flexing and often high current to ensure reliable rotation of the turbine’s nacelle.
Offshore Wind Cables Specialized power and control cables designed for subsea or highly corrosive marine environments. These cables must withstand saltwater, constant motion from waves, and extreme pressures. Their durability is critical for the long-term operational integrity and cost-effectiveness of offshore wind farms.
Direct Burial Cable A cable designed with extra-tough jacketing that allows it to be buried directly in the ground without conduit. In large wind farms, direct burial saves significant costs on trenching and conduit. The cable’s jacket must be resistant to moisture, chemicals, and rodent damage to ensure longevity.
SCADA System (Supervisory Control and Data Acquisition) A control system architecture that monitors and controls industrial processes, including entire wind farms or solar plants. Cables are the backbone of SCADA, transmitting critical sensor data and control commands. Reliable communication cabling is essential for remote monitoring, optimizing performance, and responding to issues in real-time across a large energy site.
MV/HV Cables (Medium Voltage / High Voltage Cables) Power cables designed to transmit electricity at higher voltages, typically from the wind farm’s collection points to the grid substation. These robust cables are essential for efficiently transmitting large amounts of power over long distances within the wind farm and connecting it to the main grid, minimizing energy loss.
Armored Cable A cable with an added layer of metallic protection (e.g., steel tape or wire armor) beneath the outer jacket. Used in wind farms for direct burial or in areas where cables are vulnerable to physical damage (e.g., from machinery, rodents, or construction). The armor protects conductors from cuts, crushes, and abrasions.
Rodent-Resistant Cable Cables designed with materials or structures (e.g., glass yarns, tough jackets) that deter rodents from chewing through them. In outdoor wind farm installations, rodents can cause significant damage to cables, leading to outages. Rodent-resistant cables protect against this common threat, ensuring continuous operation.

For Energy Storage System (ESS) Integrators & Managers

These terms are crucial for battery energy storage systems, from small commercial setups to utility-scale grids.

Term A Simple Definition Why It Matters for Your Project
Battery Cable High-current DC power cables used to connect battery modules, racks, and inverters within an energy storage system. These cables carry very high DC currents and must be sized correctly to prevent overheating and power loss. They often require specialized insulation and connectors for safety in compact, high-power battery environments.
DC Disconnect Switch A safety device used to manually or automatically disconnect the DC power flow from a battery or solar array. Proper cabling to and from this switch is vital for system safety during maintenance or emergencies. High-quality cables ensure minimal resistance and reliable operation of the switch.
Grid-Tie Inverter An inverter specifically designed to synchronize with and feed power directly into the electrical grid. The AC output of a grid-tie inverter requires robust, properly sized AC power cables to efficiently and safely deliver power to the utility grid, often under strict regulatory requirements.
Conduit (Electrical) A tube or pipe used to protect electrical wiring, typically made of metal or plastic. While some cables are direct burial, conduit provides an extra layer of physical protection against damage for critical power and communication cables within an ESS site.
Fire-Resistant Cable Cables designed to maintain circuit integrity and continue functioning for a specified time during a fire. In dense battery storage facilities, fire safety is paramount. These cables ensure critical monitoring and suppression systems remain operational during an emergency, buying valuable time for intervention.
BMS Cables (Battery Management System Cables) Specialized communication and signal cables used to connect battery management systems to individual battery cells or modules. These cables transmit vital data on battery voltage, temperature, and current, ensuring safe operation, optimizing charging/discharging, and extending battery lifespan. Reliability is critical for preventing thermal runaway.
Fiber Optic Patch Cables Short lengths of fiber optic cable with connectors on both ends, used for connecting devices within a data network. In ESS facilities, fiber optic patch cables provide high-bandwidth, noise-immune connections for SCADA systems, remote monitoring, and data logging, essential for managing complex battery arrays without electrical interference.