Skip to content
Lapp Asia Pacific SG
Spend SGD 1,200 more for FREE shipping.
FREE shipping will be applied at checkout

Your cart is empty

Continue shopping
0Cart(SGD 0.00)

EPIC® M23 Connectors: The Workhorse Connector for Industrial Automation

What happens when a servo connector loosens halfway through a production shift? A line stops, an axis loses position, and a technician opens a control cabinet during peak output. EPIC® M23 connectors are the 23mm circular connectors built for that problem. They sit in servo motors, feedback systems, and motion-control applications where secure locking, dense pin layouts, and reliable contact under continuous vibration are non-negotiable. M23 ships in SIGNAL, POWER, and application-specific insert variants, with exact contact count, current, voltage, IP rating, and mating cycle figures tied to the insert, housing, and termination chosen. For the part you have in mind, confirm specs against the LAPP SEA eShop M23 listings and the EPIC® Circular Connectors Guide.

For machine builders and automation engineers across ASEAN, the M23 form factor has earned its place as a widely used connector format for industrial motion control. It is sized for the high pin counts that servo systems need, engineered for the vibration profiles of packaging lines and semiconductor handlers, and integrated with cables that ship under the same engineering envelope. LAPP designs and manufactures both cables AND connectors, so an EPIC® M23 connector specified for a servo project comes from the same engineering team as the ÖLFLEX® SERVO cable terminated into it.

What Makes the M23 the Right Connector for Servo Motors?

Servo motors have a specific cabling problem. They sit at the end of high-flex drives that vibrate continuously, they handle both power and feedback signals, and they live inside enclosures where space is tight and EMC requirements are real. The M23 form factor was developed for that environment. The 23mm circular housing locks securely under vibration, holds insert configurations dense enough for multi-channel signal and power, and is built to ride continuous motion cycles.

Three things separate EPIC® M23 from generic circular connectors. The threaded coupling holds contact integrity through repeated motion cycles, which matters when an axis is reversing thousands of times per shift. A single M23 housing accepts different insert configurations for SIGNAL, POWER, and combined applications, so one connector family covers most of a machine builder’s motion control stack. EPIC® M23 components are selected with reference to IEC 61984 requirements, with approvals and ratings confirmed on the specific part page in the LAPP online catalogue.

For semiconductor handlers, packaging lines, and intralogistics machines across ASEAN, those three factors are why M23 is widely used.

How Do You Choose Between EPIC® SIGNAL and POWER M23?

The SIGNAL versus POWER decision is usually clearer than it looks. The question to ask first is what is flowing through the cable.

EPIC® SIGNAL M23 is built for high pin density at lower current. Feedback signals from encoders and resolvers, low-current control lines, and digital communication buses run cleanly through SIGNAL inserts. If your application is feedback or signal, SIGNAL is the answer.

EPIC® POWER M23 is built for fewer pins at higher current. Servo motor power lines, drive output stages, and three-phase motor connections run through POWER inserts. If you are moving real current to a motor, POWER is the answer.

Where it gets less clear is hybrid applications. Some servo systems carry power and feedback on a single cable run, and the choice between separating them into two M23 lines or combining them into a hybrid insert is application-specific. The EPIC® Industrial Connectors APAC overview sets out the variants, and for a borderline case our engineering team in your region can confirm which insert pairs with your motor and drive combination.

Cables and Connectors From One Source: Pairing M23 with ÖLFLEX® SERVO and ETHERLINE®

The benefit of buying both cable and connector from LAPP shows up most when the connector terminates onto a high-flex cable. ÖLFLEX® SERVO cables are engineered for the bending and twisting cycles of servo applications, and ETHERLINE® cables support Industrial Ethernet communication in automation systems. When the connector and cable come from the same source, the strain relief geometry, conductor cross-section, and shielding scheme are designed against the same reference, not assembled across two suppliers’ tolerances.

For an ASEAN machine builder, that single-source pairing reduces three sources of project drag. Sourcing time, because one engineering contact handles connector, cable, and assembly inquiries. Specification risk, because cable cross-section and connector contact rating are checked against the same dataset. And lead time, because LAPP SEA holds regional stock for both EPIC® connectors and the ÖLFLEX® cable variants commonly specified for motion control.

Browse the LAPP SEA eShop for ÖLFLEX® SERVO cables and ETHERLINE® options to scope what is in stock against your design.

What IP Rating and Mating Cycles Should You Specify?

This is where many connector specifications go wrong. There is no single ‘M23 IP rating’ or ‘M23 mating cycle figure’ to quote, because both depend on three things: the insert, the housing, and the termination type. A mated M23 housing on the machine side may carry one IP rating; the same insert with a different cable gland may carry another. Mating cycle expectations vary depending on contact plating and termination quality.

The right way to specify is to start from the application. What is the worst environmental exposure the connector will see? Pressure washdown, splash, occasional dust, or immersion. That defines your minimum IP target. How often will the connector be mated? A connector on a sensor that gets serviced quarterly is a different specification from one inside a daily-changeover tool stand. And what termination is your assembler comfortable with? Crimp, screw, or solder all have different cycle envelopes.

With those three answers, the LAPP online catalogue for EPIC® circular connectors will point you to the exact part variant that matches, and the per-SKU datasheet will give you the verified IP and mating cycle figures. EPIC® M23 housings reference IEC 61984 for industrial circular connectors. The certification details that apply to your part are confirmed on the catalogue page, not in a single article-level claim.

Talk to Our Engineers

If you are specifying M23 for a servo or motion-control project and want to confirm the right SIGNAL or POWER insert, the matching ÖLFLEX® SERVO or ETHERLINE® cable, and the assembly approach, talk to our engineers. We can size the connector, cable, and termination together for your application, with regional inventory and engineering support from LAPP SEA across Singapore, Malaysia, Thailand, Vietnam, Indonesia, and the Philippines.

Reach the LAPP APAC team at e.lapp.com/apac/contact, or browse the EPIC® M23 listings in the LAPP SEA eShop to start the specification conversation.