Skip to content
Lapp Asia Pacific SG
Spend SGD 1,200 more for FREE shipping.
FREE shipping will be applied at checkout

Your cart is empty

Continue shopping
0Cart(SGD 0.00)

Intralogistics Connectivity: Keeping ASRS & AGVs Running 24/7

It’s 3:00 AM. Red lights flash across the floor of a massive warehouse. A shuttle in the Automated Storage and Retrieval System (ASRS) has frozen mid-aisle. Within seconds, pallets start piling up on the conveyors, and a fleet of Autonomous Guided Vehicles (AGVs) sit idle, waiting for instructions that never arrive.

The line is down. Later, the finance controller does the math: every minute of that stoppage cost the company over $5,000.

Maintenance finds the culprit deep inside a cable chain: a standard network patch cord—the same kind that connects your desk PC—twisted, bent, and stretched millions of times more than it was ever designed to handle. They replace it, the line restarts, but the nagging question remains: will it happen again tomorrow night?

The Real Reason Your Automated Warehouse Fails

This isn’t a freak accident; it’s a symptom of a massive disconnect. The warehouse automation market in Southeast Asia is exploding, projected to grow at nearly 15% a year. But many facilities are still using cables that weren’t built for the ruthless, 24/7 reality of modern intralogistics solutions.

Here’s the abuse your cables actually endure:

  • Constant Bending: In the tight cable chains of a stacker crane, cables are bent and straightened hundreds of times an hour. Standard PVC jackets will crack, and the copper cores inside will fatigue and break.
  • Violent Twisting: Inside the mast of an AGV, cables are subjected to continuous torsion. A standard cable might fail after less than a million cycles, but a true motion-rated cable is tested to survive well over 10 million torsion cycles.
  • Electrical Noise (EMI): The powerful motors driving your conveyors create a huge amount of electromagnetic interference. Unshielded cables pick up this noise, leading to corrupted data packets and phantom error messages that stop your line for no reason.

The lesson is brutal and simple: in a 24/7 automated facility, your uptime lives or dies inside the moving cable.

The Fix: Motion-Rated Cables for 24/7 Uptime

To stop the 3 AM alarms for good, you need to match your intralogistics connectivity to the job. It’s not about one magic product; it’s about building a reliable system with three key components.

1. For Reliable Power: ÖLFLEX® CHAIN

Your motors and actuators need clean, uninterrupted power. ÖLFLEX® CHAIN high-flex cables are specifically designed with a fine-strand copper conductor and a durable PUR outer jacket to withstand millions of bend cycles in a cable chain without failing.

2. For Flawless Data: ETHERLINE® PN FLEX

This is your solution for Industrial Ethernet in motion. ETHERLINE® PN FLEX cables have a robust construction that protects the sensitive data pairs from the stress of constant movement, ensuring you don’t suffer from signal loss or phantom network errors.

3. For High-Speed Vision: HITRONIC® TORSION

Many AGVs and robotic systems rely on fibre optics for high-bandwidth cameras. HITRONIC® TORSION fibre optic cables are built to handle the intense twisting motions inside robotic arms and masts, protecting the delicate glass fibres from damage.

The Smartest Solution: Pre-Assembled Cable Harnesses

The best way to ensure reliability is to eliminate on-site installation errors. Instead of shipping loose reels of cable and boxes of connectors, a pre-assembled and factory-tested harness is the gold standard for ASRS and AGV systems.

This is exactly the approach taken for the massive Terminal 3 baggage handling system at Frankfurt Airport. The builders, SEAP Automation, knew that on-site termination of thousands of connections was a recipe for delays and errors. Instead, they ordered over 2,100 pre-assembled harnesses from LAPP. These systems, containing 85 kilometers of ÖLFLEX®, ETHERLINE®, and UNITRONIC® cables, arrived on-site, pre-labeled, polarity-checked, and ready to be plugged in. This approach dramatically reduced installation time and ensured that every single connection was perfect from day one.

Your Quick-Spec Checklist for ASRS and AGV Cabling

Use this checklist to make sure you’re ordering the right connectivity for your automated systems.

  • Motion Profile: Log the maximum bend radius, travel distance, and twist-per-minute for each machine.
  • EMI Zone: Are your data cables running alongside high-power motor drives? If so, you need shielded cables to prevent interference.
  • Chain Fill: Don’t stuff cable chains more than 60% full. Leave space for air to circulate and for cables to move freely.
  • Fire & Export Code: If your machines are being exported, ensure your cable assemblies are UL-certified. For fire safety, default to LSZH (Low-Smoke, Zero-Halogen) jackets.
  • Spares Policy: Don’t wait for a failure. Stock one complete, pre-assembled harness for every ten critical moving systems for a rapid swap-out.

Straight Answers to Tough Questions (FAQs)

Is a motion-rated Cat.6A cable really that different?

Yes. It’s night and day. A motion-rated cable is built with finer copper strands, a different core structure, and a tougher jacket. Lab tests show it can survive 10 million or more flex cycles, while a standard office cable often fails before it even reaches 1% of that.

We’re not a giant corporation. We can’t afford sky-high cable prices.

Downtime is always more expensive than premium cable. At over $5,000 a minute, a single 30-minute outage costs $150,000. That single event completely dwarfs the price difference for an entire set of reliable, pre-tested harnesses.

Our technology changes every year. Won’t we just have to re-cable anyway?

Not if you plan ahead. Using hybrid power-and-data cables and modular connectors means your physical backbone stays the same. When you upgrade a sensor or a drive, you just swap the device, not the entire cable run.

The Bottom Line: Automation That Actually Runs 24/7

When every pallet and every package counts, your success comes down to one thing: keeping the red lights from flashing. Investing in motion-rated, plug-and-play intralogistics connectivity takes cabling off your worry list and delivers what you were promised:

  • 10x or more flex-life compared to standard office-grade cords, preventing failures in ASRS and AGV systems.
  • Up to 70% faster installation on new lines with pre-assembled harnesses, so you can start generating revenue sooner.
  • A dramatic reduction in the unplanned downtime that kills your profits.

Don’t wait for the next 3 AM alarm. Book a 30-minute Intralogistics Connectivity Audit today. Our engineers will help you map your motion profiles, quote a plug-and-play harness, and hand you a spec sheet so you can finally get a good night’s sleep.